Murrelektronik

You are here: Home / Company / Ecology

Environmental protection

Sustainable development and long-term protection of man and nature

Murrelektronik is committed to the objectives of environmental protection. Special emphasis is given to the protection of employees and customers. This begins with the selection of raw materials: no material hazardous to health is used for the production of Murrelektronik products, as prescribed by the Dangerous Substances Directive. Lead-free production is of special importance: Murrelektronik follows the guidelines of the RoHS directive. This is also taken into account when selecting suppliers.

The very modern production facilities are designed to use less energy. Environmental criteria are also considered for shipping our goods. Only recyclable materials, such as polythene wrap and cardboard boxes are used as packing material.

Worldwide representation

Worldwide representation

Murrelektronik values connections. You will find knowledgeable contacts in our local branch offices and partner companies – worldwide.

more

Upcoming trade fairs

Elektro Vakbeurs

06.03.12 - 08.03.12
Venray, Netherlands

SIAF 2012

07.03.12 - 09.03.12
Guangzhou, China, Booth: 3.2/A135